Haydock - A Super Servo Service

Have you ever considered how your metal cutting machines create that precise motion for milling or bending those perfect lines in hard surfaces during metal fabrication processes? The answer, a specialised Servo Motor.

Distribution and Engineering Regional Hub

Firstly, let us differentiate between a traditional AC motor and a servo motor. Unlike a traditional AC motor, which does not comprise of a particular assembly, a Servo motor is made up of a magnet rotor, stator and a feedback device used for position and control. The feedback device is set up in a precise position and when the motor is taken apart and put back together, the feedback device will need to be put back to exactly where it was originally taken – they are most commonly used in closed-loop systems.

Designed to rotate specific parts of a machine with accuracy and efficiency, a servo motor is controlled with an electric signal, which can be either analogue or digital, to determine the specific amount of movement required. For example, think of a paint line at a car manufacturing plant, where the motor only needs to move a certain distance to cover its required course, with an encoder serving as a sensor that determines speed and position feedback.

As you can appreciate, operating with such complex machinery often comes with its own problems. So, when errors do arise, it’s good to know that companies such as Rubix Industrial Services have the technical expertise to provide an impartial solution that will get your production back running to its most efficient.
 

Test, repair, overhaul – The choice is yours

At Rubix Industrial Services, we are committed to providing only the highest quality of repairs, whether that be traditional motors through to servo motors.

Our approach remains, and has since day one, that any repair or refurbishment request will be returned ‘as good as new’ ensuring that your production line will be as efficient as ever before.

Servo motor repair and testing is a specialist service that requires skills in electrical, mechanical, and electronic disciplines – a combination of skills difficult to source in today’s industry.

Backed by an experienced team of engineers with decades of knowledge and expertise,  Rubix Industrial Services offers an unrivalled servo motor repair service out of our specialist Haydock Regional Hub.

With the capabilities to offer support with spindle motors, water-cooled generators, AC / DC servo motors, Rubix Industrial Services repair capacity includes:

      • Bespoke servo motor/repair cell
      • Complete fault assessment
      • Full overhaul and rewind capabilities
      • Motors stripped, tested, and aligned using
      • a Mitchel TI-5000
      • Encoders including SICK (SRS, SRM),
      • Heidenhain (ERN, EQN) and Tamagawa
      • Resolvers
      • Hall effect sensors
      • Tachometers

 

Haydock - A Super Servo Service

Unsure of specification?

With a small yet dedicated team of three specialist servo motor engineers, our Haydock facility also has the expertise and skillset to reverse engineer components utilising data sheets that are readily available online.

This means that even if you’re unsure of the correct specification for your application, our engineers can source the blueprints you need and ensure that your servo motor matches any requested specification.

Utilising an unrivalled support network, Rubix Industrial Services is proud to offer a 24/7 servo motor service, with an anytime call-out option, with geographical coverage capturing the entire UK. Add that to our renowned impartiality, and whether it be a simple test, complex repair, or complete overhaul, we’ll get your production line back up and running in no time.


For more information on our expert Servo Motor capabilities or to make an enquiry, contact your local Local Branch, who will be happy to discuss your options.

#Engineering #Repair #Supply #Haydock

Author

Mike Golds

Mike Golds

Mike started his 42 year engineering career at Mather and Platt as a technician apprentice, going on to become a commissioning engineer.....
More...

A career change into the water treatment and construction industry provided new experiences and knowledge which enabled a step change into senior leadership with Weir Engineering Services, Flowserve and Celeros Flow Technology enjoying roles within sales and service operations in the UK and Middle East for over 25 years.