Blog - Engineering Repair Replace

A record rewind for Rubix Industrial Services Chesterfield

When a complex alternator stator at a major refinery required a rewind, the customer didn’t pause. They wanted a partner with the experience, expertise and resources to meet the challenge. And that’s where Rubix Industrial Services' know-how came into play, to complete the project in record time.

multiple rewind video symbols on a blue background

The stator is part of a customer’s generator, driven by steam from the refining process. After several decades of service, it was at the end of its life and at risk of failure. It was already producing high partial discharge in service. To rewind it would be a 3-month project, but manufacturing new coils beforehand would normally take an additional 6 weeks. With the generator out of action for so long, the customer would have to buy in their energy, with significant cost implications.

Fortunately, Rubix Industrial Services’ forward-planning and rewind capabilities helped to save the client time and money.

Here’s one we made earlier…

The customer’s stator is not a standard design. It incorporates unconventional coils of a complicated shape, that demand special tooling and jigging for their manufacture. This all helps to increase the cost and the lead time.

Fortunately, Rubix Industrial Services' had manufactured replacement coils for the customer several years before. They were stored in special crates, inside sealed foil bags with a desiccant, and all ready to be used immediately.

Rubix Industrial Services' understanding of the stator, gained during the manufacture of the coils, made them the obvious choice for the rewind. But it was a rewind with nothing obvious about it.

A stripped stator alternator

Stator stats.

A typical stator has a diamond coil winding, which is relatively straightforward to rewind. This one was far from typical and far from straightforward.

The individual coil bars forming the winding are fanned out at the end winding, with each bar end required to be manually formed, joined and connected, to complete the winding and create the 3-phase, 2-pole circuit.

The stator consists of 60 slots, with a top and bottom bar in each slot. Each of those bars has 2 conductor turns, and each conductor turn comprises 10 parallel copper sectional strips.  That’s a total of 2,400 individual sectional strips running through the stator and protruding at each end – making 4,800 copper strip ends in all.

Each of these ends has to be individually shaped – a process requiring care, precision and skill – then cut to size, braze joined, insulated by hand, and formed into the individual conductor turn. The completed and formed noses then have to be over-insulated, and all the associated end-winding supporting and bracing structure also has to be formed and secured.

It’s clear why the whole rewinding process took even Rubix Industrial Services’ experienced engineers 10 weeks of round-the-clock working.

Rewind re-think

When the alternator stator had last been rewound, the only insulation available was Class B rated.  Many years on, the availability of Class F insulation enabled Rubix Industrial Services to propose an upgrade.

The gearbox rewind with coils and varnish

The thinner insulating material meant there would be enough space to accommodate conductive ripple spring side packing to secure the coils in their slots. This ensures more effective prevention of partial discharge in service and securing of the coils.

The customer agreed, and the stator was rewound to the new, higher standard for even more effective performance. But even so, nothing was left to chance.

A test at every turn

A battery of tests was carried out throughout the rewind process, and once it was completed, to eliminate any potential mistakes and guarantee the quality of the operation.

These tests included:

  • low resistance tests to check for poor joints
  • circuit resistance balance tests
  • polarity tests
  • inter-turn tests
  • a variety of insulation tests.
 

Lastly, before the rewound stator was approved to leave Rubix Industrial Services’ workshop, it was subjected to a one-minute HV withstand test at 23,000V, followed by partial discharge and tan delta tests.

Put on the spot

The customer’s operating environment – a major oil refinery – is clearly a volatile one, with numerous associated health and safety risks. So to carry out the rewind, the alternator stator was transported from the customer’s site to the Rubix Industrial Services workshop, where it was stripped and rewound before being returned to the refinery for installation.

However, the customer was sufficiently impressed by the conduct and capabilities of Rubix Industrial Services’ engineers in the workshop that a second job has now been booked. And to eliminate the time, complexity and cost of transportation, this time Rubix Industrial Services will be working on-site.

Meanwhile, the successfully rewound and generator alternator stator with its upgraded insulation is back in operation, with a service life confidently expected to equal that of the plant.

With few suppliers able to match their experience, expertise or resources, it’s clear that Rubix Industrial Services should be the first choice for a rewind of this scale and complexity. And you can put that on record.


For more information on Engineering, Repair and Replace solutions , please contact your Local Branch, who will be happy to discuss your options.

 

#OilRefinery #Engineering #Insulation 

Author

Trevor Hilton

Trevor Hilton

I joined Rubix Industrial Services in January 2013 in an external sales role at the Chesterfield branch, concentrating on customers requiring small and medium voltage motor repairs
More...

Three years ago I took up the position of High Voltage Sales and Development Manager at Chesterfield, with the task of increasing the number of customers for which we provide High Voltage motor repairs, overhaul, inspection and monitoring to..

Prior to joining I spent 16 years working for both Tsubakimoto and Renold Chain in customer service sales, moving to Sales Supervisor, Sales Office Manager, European Sales Office Manager, and UK Key Account Sales.
I am married to Sandy, and have four children, Mathew (aged 22), Aaron (aged 20), Isaac (aged 17), and Aaliyah (aged 16). My family take up the majority of my spare time, but I try to get on the golf course most Saturday mornings.

I am also a keen walker and enjoy wandering round the local nature reserve in Nottingham with our dog. I also take infrequent trips to the gym, and enjoy watching most sports from the sofa.